10/23/2013 11:13 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question splitted to PLC S7-315-2PN/DP can be programmed by PCS7 also, is it true? Best regards O_Moderator |
2/8/2016 4:27 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Lucky123 is split to a separate thread with the subject PCS7 example with Indl Lib. Best regards |
2/9/2016 10:01 AM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
You can engineer the 300 CPUs, which are in the PCS 7 hardware catalogue, like the 400 CPUs, that is right. But you have to use the blocks from the S7 Industry Library not from the PCS 7 Industry Library. Both Libraries are on the Industry Library DVD for PCS 7.
|
SIMATIC PCS 7 - Overview |
|
Follow us on