5/30/2014 1:05 PM | |
Posts: 4 Rating: (0) |
Hi, Thanks a lot. I will try it out and will let you know. Thanks and Regards, BM |
6/3/2014 12:11 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1423)
|
you are wellcome :) |
Denilson Pegaia |
|
2/26/2017 1:50 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello,
With the function VAL_STR you can convert numerical values in the PLC to ASCII strings. Once you have the databloc with the right structure, next step is to send the DB as a file using FTP (file transfer). |
Best regards |
|
3/1/2017 8:45 AM | |
Joined: 1/30/2006 Last visit: 4/2/2024 Posts: 310 Rating: (57) |
Hi Try to see this Brand New Application Example. The example saves .csv. files on a local computer, and it should be easy from here either to write a parser in VBA or simply import the datasources into Excel TCP File Server for S7 Controller BR. Sven |
BR. Sven |
|
This contribution was helpful to2 thankful Users |
Follow us on