10/15/2009 2:49 PM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi carmamezo , if you are using PCS7 the operation log is automatically carried out without write any script. for I/O editing field directlry from graphic rutime just select "Operator Activity Report = YES" for set/reset bit by pushbutton it possible check box "Operator Input message" from mouse action in Direct Connection. Any changes from faceplate are automatically carried out in "Operation List" messages. Hope can help regards AttachmentActivity Report.zip (374 Downloads) |
This contribution was helpful to5 thankful Users |
9/3/2015 11:29 AM | |
Posts: 41 Rating: (1) |
What if I have a C-action on my button? |
3/23/2017 4:25 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Awesome. With the ''operator activity report / Message' for I/O and ''operator input message'' for direct connection of a digital input, i was able to generate operator message with ease. However, further on C script or VB, anyone knows how to create the operation messages with it for digital and variable in WinCC graphic designer? Thanks for help~ |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on