11/7/2016 1:36 PM | |
Posts: 52 Rating: (1) |
Hello :) I have a problem with the communication between Simatic Mangaer and WinCC. The steps for my process: 1. Open the project in Simatic Manager 2. Make new internet connection for S7 program. (address 192.168.1.35) 3. Right click on OS and compile. 5. Chose the connection that I made. 6. Open WinCC and Tag managment. 7. Run runtime to see if the connections works. I have Simatic Manager v5.5 sp4 WinCC 7.3 For simulator I use DeltaLogic ACControl (Address of the simulator that is in use is 192.168.1.35 First time I didn't know how to change the ip address in the WInCC because it was read only. When I made this step and changed the address it was the green symbol in tag managment that indirected that the connection works. I went forward and worked on some pages, and when i decide to check my work i couldn't make the same connection. I get always the red symbol that shows that is no connection. Now I don't know what may be the problem? In attachment are pictures of the problem. AttachmentSImatic Wincc.zip (49 Downloads) |
Last edited by: deco10 at: 11/7/2016 2:18:53 PM |
|
3/24/2017 2:58 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by anlugr is split to a separate thread with the subject WinCC button takes Simatic Manager. Best regards |
Follow us on