3/24/2017 11:26 AM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (106) |
Hello all. This is my hardware equipment: This is order inside TIA selection tool: (but I'm tryinng to make program inside STEP 7 v5.5 sp4) 1. 6ES7405-0DA02-0AA0 (PS) 2. 6ES7412-5HK06-0AB0 (S7400H CPU) 3. 6ES7405-0DA02-0AA0 (PS) 4. 6ES7412-5HK06-0AB0 (S7400H CPU) 5. 6ES7153-2BA10-0XB0 (ET200M IM 153-2 ) 6. 6ES7153-2BA10-0XB0 (ET200M IM 153-2) 7. 6ES7321-1BL00-0AA0 (DI x 32) 8. 6ES7321-1BL00-0AA0 (DI x 32) 9. 6ES7321-1BL00-0AA0 (DI x 32) 10. 6ES7321-1BL00-0AA0 (DI x 32) 11. 6ES7322-1BL00-0AA0 (DO x 32) 12. 6ES7322-1BL00-0AA0 (DO x 32) 13. 6ES7331-1KF02-0AB0 (AI x 8) 14. 6ES7331-1KF02-0AB0 (AI x 8) 15. 6ES7331-1KF02-0AB0 (AI x 8) 16. 6ES7331-1KF02-0AB0 (AI x 8) 17. 6ES7332-5HD01-0AB0 (AO x 4) 18. 6ES7350-1AH03-0AE0 (FM350-1 COUNTER) This I'm trying to configure inside step 7 v5.5 sp4 I did that on this way inside STATION H, take a look picture 1 I'm able to do compile without problems. I've noticed following : Modules addresses inside (ET200M IM 153-2 for 1. PLC) and (ET200M IM 153-2 for 2. PLC) can not have same ADDRESS. Take a look picture 2. If I open each module inside properties I can choose redudancy module, so I choice appropriate module from different DP Master. Take a look picture 3. I'm able to do this for DI and DO modules, but for AI, AO and COUNTER nope. Take a look picture 4. Why is that case, am I doing anything wrong with hardware configuration? Project is uploaded here as attach, and here are links for pics: pic1 : http://i.imgur.com/1whdlCq.png pic2 : http://i.imgur.com/GAxIsI0.png pic3: http://i.imgur.com/8MLes56.png pic4 : http://i.imgur.com/32Eb7Zh.png THX in advance AttachmentHW_PROJECT.zip (162 Downloads) |
Last edited by: SOble at: 3/24/2017 11:43:25 AMLast edited by: SOble at: 3/24/2017 11:44:43 AMLast edited by: SOble at: 3/24/2017 11:47:03 AMWebsite: |
|
3/27/2017 2:32 PM | |
Joined: 6/14/2006 Last visit: 4/29/2024 Posts: 301 Rating: (60) |
Hi SOble, I think there is a misunderstanding. If you have redundant PLC and redundant profibus networks you need two times the IM153-2 inside each ET200M rack. So you have at the same backplane: Power supply | IM153 | IM 153 | DO | AO | ..... There is no need to configure two ET200M racks in hardware configuration as you see in your configuration the ET200M is connected to both Profibus master systems. The address for both 153-2 is set only once in hardware configuration. Be aware that you need a special bus module for both IM 153-2, too. I do not know the exact number but the text is bus module IM/IM. No need to do anything in the redundancy tab of DI or AI modules. This is for I/O channel redundancy only. Have a look to chapter 4.4 of this document to understand better: https://support.industry.siemens.com/cs/de/de/view/109476178/en Regards |
Follow us on