11/14/2013 11:46 AM | |
Posts: 2 Rating: (0) |
Hello, I want to use thedemo project as a template. I've downloaded the demo project from here https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=65384955&nodeid4=20229806&cspltfrm=0&cssw=0&csbinh=0&load=content&subtype=136000&lang=en&siteid=cseus&aktprim=4&objaction=csview&extranet=standard&viewreg=WW. I've followed allthe instructions in the pdf file and everything seems to be working. WinCC RThas established connection with the CPU witchI'm using, everything looks fine, WinCCarchive is making databaseandI'm able tomake powerrate reports. The problem is that there are 3 errors in WinCC: 1. S7-Program(1)/DB_ARCHIVE_B2 Communication error with ID1 2. S7-Program(1)/DB_RCV Communication error 3. S7-Program(1)/DB_SENDCommunication error The IDs are the same as in NetPro and the comunnication IDs are unique. In Step 7 inDB_ARCHIVE_B2 there is aerror inaddress 40.3 (QMSG_ERR) ALARM_DQ Error and state is FALSE for address 48.0 (MSG_ACKID1) Messages acknowledged ALARM_DQ block 1, address 48.1 (MSG_ACKID2) Messages acknowledged ALARM_DQ block2and address 48.2 (MSG_ACKID3) Messages acknowledged ALARM_DQ block 2. If I acknowledge the alarms in WinCC RTnothing change to Step 7 DB_ARCHIVE_B2 and the alarms in WinCC RTgo to status QS (red color check mark). I have no experiencewith WinCC, just WinCC flexible. As far as I understand everything in WinCC(including alarms)is made by thecompile OSwizardin Step 7, OS Project Editor and Powerrate wizard in WinCC. I think the problem is the communicationof alarmsbetween WinCC and CPU, but I don't know what to do. Please, help. |
Last edited by: Synchronize at: 11/14/2013 12:21 PM |
|
3/27/2017 2:27 PM | |
Joined: 4/13/2014 Last visit: 8/3/2023 Posts: 8 Rating: (0) |
could you provide us with solution or the steps to override this problem?! |
3/27/2017 3:09 PM | |
Joined: 4/13/2014 Last visit: 8/3/2023 Posts: 8 Rating: (0) |
Hello , I have program SIMATIC Powerrate V4.0+SP3 installed on PCS7 V8.1 but i have library SIMATIC Powerrate V4.0 + SP1 which is extracted from demo example of SP1. I have problem in block Load Management LMGM . When i open the faceplate and try to load from PLC , i receive a message "Transfer Active! . Please Wait" but then i receive an alarm "Monitoring error archiving". LMGM block will set QMONERR_S . Also , i want to know how to configure parameter ID and Arch_ID in blocks LMGM , PRE_UA_S and PRE_UA_R Attachmentattached.zip (402 Downloads) |
Follow us on