3/27/2017 3:13 PM | |
Joined: 4/13/2014 Last visit: 8/3/2023 Posts: 8 Rating: (0) |
Hello , I have program SIMATIC Powerrate V4.0+SP3 installed on PCS7 V8.1 but i have library SIMATIC Powerrate V4.0 + SP1 which is extracted from demo example of SP1. I have problem in block Load Management LMGM . When i open the faceplate and try to load from PLC , i receive a message "Transfer Active! . Please Wait" but then i receive an alarm "Monitoring error archiving". LMGM block will set QMONERR_S . Also , i want to know how to configure parameter ID and Arch_ID in blocks LMGM , PRE_UA_S and PRE_UA_R Attachmentattached.zip (24 Downloads) |
3/28/2017 8:38 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Previously i had a problem with PRE_SUM block FB1061 which come from Power Rate V4.0 SP2. The archive tags stored in alarm logging - "Pre" folder instead of System archive. After that, at WinCC, if we opened the PRE_SUM block faceplate trending, other faceplate will be unable to retrrieve their archiving record. After that, we seek advice from siemens support, they told us they had solved the issue with Power Rate 4.0 SP3. Below reply retrieved from Siemens support email sent to me previously "Based on the project which was delivered, we could see that the picture “@PG_PRE_Trend.pdl” inside this project is still the old one. The correction for this issue has been implemented in SIMATIC powerrate V4.0.2.1 and V4.0.3. After installation of the version, the corrected picture is installed on the installation drive. To copy thiecorrected picture into the project, the steps äre inside power rate released note." Im not sure whether this could help you or not, but different service pack or faceplate picture might affect the result and communication. Hope this is useful for you. |
Last edited by: JazTai at: 3/28/2017 8:39:26 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
3/28/2017 11:44 AM | |
Joined: 4/13/2014 Last visit: 8/3/2023 Posts: 8 Rating: (0) |
Thanks for your replay. Actually I'm waiting the V4 SP03, and I'll give you a feedback. Thanks |
Follow us on