7/1/2013 3:05 PM | |
Joined: 5/28/2013 Last visit: 2/1/2023 Posts: 112 Rating: (3) |
Hello, I recomendhttp://www.profibus.org/ In this website theres some articles, few videos, webinars and a lot of technical specifications.. Regards
|
7/1/2013 5:46 PM | |
Posts: 621 Rating: (10) |
Hello please check in wekipedia or www.profibus.com websites process in field bus related documents
|
7/1/2013 6:27 PM | |
Posts: 95 Rating: (10) |
Hi As I a little research about profibus ; this is a communication protocol that industrial hardware use for exchange data in industrial network. The base of profibus is that it's at first send some data to slave for known the slave devise .after slave inform itself to master ;master Send some data to slave for set the parameter in slave for example name of slave, and next master start exchange data whit slave(read input; write out put diagnostic data and …) Profibus is this rule for exchange data between master (plc for example) and slave (ET200 for example) I put some pdf file for you that I thing can help you If you need more data tell to put them for you AttachmentProfibus.pdf (340 Downloads) |
4/24/2017 3:55 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by iiui is split to a separate thread with the subject Material for completed understanding regarding profibus. Best regards |
Follow us on