4/24/2017 8:34 AM | |
Posts: 88 Rating: (4) |
Use Normx for taking the raw value from transmitter then use scale option for scaling between the required values. |
4/24/2017 9:21 AM | |
Posts: 8 Rating: (0) |
Can you explain it in detail sir plz ?? |
4/24/2017 10:10 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi You can refer the programing manual in the Step7 help catalog. On how to insert a Card, Configure the IO card in the HW configuration and programing it. You can program using LAdder as your first project, LAD Communication and other Working with Step7 Take care and take a backup of the project before you start adding and editing the program so that you can refer in case of a problem. Program safe... |
Jazz |
|
4/24/2017 2:36 PM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585) |
Hi, you can also check the following FAQ: How do you standardize and destandardize analog values with STEP 7 (TIA Portal)?Regards, Towome |
|
|
4/25/2017 11:45 AM | |
Posts: 88 Rating: (4) |
Dear Zaibkhan You can use this scale block from the attached program for your programming. AttachmentSCALE.zip (389 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on