6/8/2015 9:24 AM | |
Posts: 8 Rating: (0) |
hello , i am trying to get an modbus connection working with TCP . as an master. my slave is an Emerson (Daniel) 2350A GC (gas chromatograph) i am using an CPU 1512sp-1 PN with Tiaportal V13 sp1 latest update. and the Block MB_SERVER . (V3.0 - instructions V4.0) my DB for "MB_hold_register input", i had to tick off the "optimized block acces" setting to get it connected... " with an Modbus tool in windows i can connect with the Slave and see the data. only strange thing is that i configured the Slave to start on 47001 adress (holding) and i have to set my tool to start at 47002. to get it working . but the data isnt shifted. " the slave sends out 11 reals , and the Indianness is differnt with siemens (i know for a fact) so maybe thats caused the offset for 1 register. ive added an word document with all the screenshots how ive programmed in tiaportal and how i configered the slave (GC) and the windows tool. hopefully you can point me to a setting maybe in an DB that i made wrong or did not make at all. I've used an example programm from this forum to get started. ps i know for a fact that the Emerson GC is a different ENDIAN so the Reals get word swapped when i receive them . maybe i have to do somthing with that . with my parameters. i know how te swap them after i get the data btw... thanks in advance. christian van putten.
AttachmentMB_SERVER CONNECTION EMERSON GC.docx (197 Downloads) |
Last edited by: christian.vanputten at: 6/8/2015 9:38:05 AM |
|
6/8/2015 9:41 AM | |
Posts: 8 Rating: (0) |
Hi , thanks for the info . I will try that now , if i get it working i will let it know here. |
Follow us on