4/27/2017 6:39 PM | |
Posts: 5 Rating: (0) |
Hi, I am using S7200 Smart ST 20 CPU. I am making a logic in which i need to use around 70 bytes of M/Flag Memory. Can do that...?? Because, When I address the NO contact from M0.0 to M31.0, it works fine but from M32.0, a red underline comes the address, Indicating that something is wrong. What does this mean? How can I resolve this? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/28/2017 12:59:27 PMNew subject after splitting |
|
4/28/2017 3:51 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2685) |
Hello susmis; To add to the information provided by Duris, all the S7-200 SMART CPUs seem to provide a total of 256 bits (32 bytes) of M-memory. However, they also provide V-memory, up to 8 kbytes, that you can access in bit ( or byte, or word, or Dword) format through your program; in the example they show V10.2 as a valid bit address. So you could use V-bits in replacement of the M-bits you wanted originaly with the same functionnality. See the following screenshot, taken from this manual: Hope this helps, Daniel chartier |
Last edited by: dchartier at: 4/28/2017 6:28:08 PMLast edited by: dchartier at: 4/28/2017 8:00:31 PM |
|
This contribution was helpful to1 thankful Users |
4/30/2017 2:29 PM | |
Posts: 5 Rating: (0) |
Hi. Thanks for your guidance Danield and Duris. It works now. Thanks agains. |
This contribution was helpful to1 thankful Users |
Follow us on