Industry Online Support
Technical Forum
6/27/2013 2:31 PM | |
Posts: 72 Rating: (2) |
hi, all ready this topic has been discussed by the experts and please refer the link
|
6/28/2013 7:19 AM | |
Joined: 10/3/2010 Last visit: 3/14/2024 Posts: 1552 Rating: (188) |
In theory, you can open a WinCC project from WinCC Flexible. It will start the Migration Wizard. Mainly, it claims to only convert tags and screens but last time I tried this, I use Flexible 2008 SP3 to open a WinCC V7 project. Migration works only up to WinCC V6.2.Often the result of migration is too limited and disappointing. Projects created in WinCC V 6.2 can be migrated to WinCC flexible. However, only a few Brgds. |
Last edited by: SteBo at: 6/28/2013 7:21 AMB r g d s , |
|
This contribution was helpful to1 thankful Users |
5/2/2017 12:44 PM | |
Posts: 50 Rating: (3) |
It is not possible to migrate/ convert the wincc project to the Wincc flexible project. |
Follow us on