5/16/2017 3:28 PM | |
Joined: 7/21/2010 Last visit: 4/24/2024 Posts: 46 Rating: (5) |
HI Experts, we have an issue with a machine at our customer in Thailand, sometimes simotion goes to Stop after and Emergency stop is triggered. We have an S7-1500 with Simotion D435 which are connected by IO Device on X150 Emergency circuit is hardware (Pilz) and is triggering STO on the drives. 4 more CU320 are connected by Profinet IRT on X150. We see a lot of errors 20005 errors and an IPO task timeout, but we have no clear idea what's the best way to solve this. Any help would be greatly appreciated AttachmentDevice Diagnostics_stopped.zip (76 Downloads) |
Follow us on