5/25/2017 1:34 AM | |
Joined: 6/28/2013 Last visit: 9/12/2023 Posts: 3 Rating: (0) |
I am having a problem after performing a general reset on 840C control. When I load the tea3 file the drive config loads and is accepted ok. When I try to load the drive MD I get 165033 Conversion Has Not Been Switched off. I have repeated the process several times with several different tea3 files and get the same results. I know if a boot file already exists I will get this error but I am unsure how to check if the boot file has been deleted during the drive general reset process. I have also tried to change the Drive MD individually for the FDD or Motor/PS data, which currently has all "*" in MD, and when I enter a value I get the error message "IC error 76 data not accessible at present". Can someone tell me what the IC error message is and provide some feedback for loading the drive MD. I have read the alarm description for 165033 and tried the steps it suggests. Thanks! Dan Attachmentsystem pics.zip (38 Downloads) |
Last edited by: Majors at: 5/25/2017 2:14:39 AM |
|
Follow us on