5/18/2017 12:13 PM | |
Joined: 8/11/2010 Last visit: 2/20/2022 Posts: 30 Rating: (2) |
Hi experts, My situation is like this. I had PC station ran under Windows 7 and configured with Simatic Net 8.1 and NCM 5.5 SP2. Everything was perfect. Then Windows OS was upgraded to 10 and I installed Simatic Net 13 SP2 to ensure workability of the station. The problem appeared as soon as OS was upgraded and was not eliminated with Simatic Net upgrade - station manager tries to load station configuration and finishes the process with error (pic_1 and pic_2). After confirmation I can open station manager but there is no station configured and all buttons disabled (pic_3) I had reinstalled Simatic Net but it did not help. Please suggest any solution to make the station running. Attachmentpics.zip (35 Downloads) |
5/24/2017 10:53 AM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1641) |
Hello ygus yes i had a similar Problem but you could download the ALM Version in the link you could use with Win10: https://support.industry.siemens.com/cs/de/en/view/114358 It works for me. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on