9/30/2016 8:17 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
In this topic you can find a document how to set up the SIMATIC IOT2000 the first time. After working through this document you can go on with the "SIMATIC IOT2000 Getting Started" to create your first project. Feel free to share your experience with this Setting up! Update 04.02.2020: Update 16.01.2017: AttachmentSIMATIC_IOT2000_Setting_up_V2.6.pdf (7597 Downloads) |
Last edited by: bergmanu at: 9/30/2016 9:11:28 AMadded link and document Last edited by: bergmanu at: 9/30/2016 11:34:23 AMedit document Last edited by: bergmanu at: 9/30/2016 11:43:34 AMLast edited by: bergmanu at: 1/16/2017 2:46:07 PMchanged document - from V1.0 to V2.0 Last edited by: bergmanu at: 8/31/2017 3:24:13 PMchanged document version from V2.0 to V2.1 Last edited by: bergmanu at: 12/8/2017 7:30:18 AMcorrected error: /etc/network/interfaces instead of /etc/networking/interfaces to change IP adress Last edited by: bergmanu at: 02/04/2020 14:52:00updated document to V2.6 Last edited by: bergmanu at: 02/04/2020 14:53:02Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to7 thankful Users |
2/7/2017 11:04 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi shamu2000, Siemens now has its own Plug-In and SDK for Eclipse. Please refer to the Getting Started V2.0, there you can find the links to download and an instruction how to use. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
2/27/2017 10:02 PM | |
Posts: 1 Rating: (1) |
Download Reference #30.6fdf02cc.1488226738.1dd58de4
Just setup logon information nd confirmed email. Is there a waiting period? |
This contribution was helpful to1 thankful Users |
2/28/2017 6:45 PM | |
Posts: 1 Rating: (0) |
I got the same error after registration. One day later I could download the file. |
5/26/2017 3:45 PM | |
Joined: 7/25/2014 Last visit: 5/3/2024 Posts: 6 Rating: (0) |
Hi folk, can i and how to install webmin on iot2000? Simone |
5/29/2017 10:42 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, yes you can install webmin on your IOT2000. Therefore you have to build a image by yourself including webmin. Here you can see the layer where webmin is included. How to build an image please follow the instructions and the link to github in this post. For including webmin you have to do the following additional steps to the meta-iot2000-example readme: 1. Add the layer to bblayers.conf:
2. Add webmin to the example image: Edit the file poky/meta-iot2000/meta-iot-example/recipes-core/image/iot2000-image.inc and add:
After adding these two files and building the image webmin is included in your image! Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on