6/8/2017 8:16 AM | |
Posts: 11 Rating: (0) |
Experts! Need Help In My application i have Siemens CPU 316 WITH APPROX 28 PROFIBUS NODES (including Simovert Master Drive -14N.o.s & IM153 & Et200 Module).There are 02 Drives which are running with Single slection from HMI and drive were running normally for weeks but sudden 01 SImovert Master is creating Problem after Enabling. Problem Detail:Normally drives shows P008 and after enabling one drive is running normally(5.4 Hz approx) while other is showing some values for 1-2 second on Drive Display & slight Movement Physically then stuck or showing 0.000 on display ,mean while other drive is running normally. Kindly guide me what would be the possible cause for this Drive response problem Task Atempted:Re parameterize drive again but status is same Changed CUVC card -Reparameterize -Status same Checked Profibus shield Grounding -OK Checked Drive Power DC Link -OK -Motor Check OK Plc status: normal no bus/Communication failure.-Online Status Drive status Normal Drive Model #:6SE7023-8TD61-Z Communication card :CUVC + CBP +T100 Siemes CPU 316 Attached Simover Mster Drive Wiring Diagram System Topology-Profibus nodes. Thanks AttachmentSimovert Master Drive Wiring And Profibus.pdf (140 Downloads) |
Follow us on