6/22/2017 2:57 PM | |||||||||
Posts: 648 Rating: (95) |
Dear dhawal, this isn't normal behaviour. If you connect a drive without an external power supply which needs more current as the USB plug can give, the panel will made a reboot. You can solve this problem if you connect a drive with an external power supply. An Alternativ can be to use a usb hub with external power supply. More information you can find under the FAQ "Which Hardware can be connected to the USB port on HMI operator panels"
With best regards rh1990 |
||||||||
Follow us on