6/23/2017 11:37 AM | |
Posts: 1 Rating: (0) |
Hello, I'm having some issues with the configuration of a module SICK POMUX KH53 and recieving the information through Profibus on a S7-300 PLC.. I've downloaded the GSD file from the manufacter, installed it and configured my module to recieve information through the Profibus. But the problem is that i do not know what are the wrong paramaters that i introduced and which are the good ones. The CTRL+D on the Profibus DP Module of KH53 is giving me a wierd error that i cannot understand. Perhaps you can help me out ! Here is an image of the configuration of the moldule : Best regards, Attachmentpictures.zip (32 Downloads) |
Last edited by: Claude_David532 at: 6/23/2017 11:38:13 AMLast edited by: Jen_Moderator at: 6/23/2017 2:41:04 PMUpload images |
|
3/14/2018 7:23 PM | |
Posts: 2 Rating: (0) |
Hiiii Is your problem solved. |
Follow us on