6/25/2017 5:32 PM | |
Joined: 9/27/2006 Last visit: 5/4/2024 Posts: 12257 Rating: (2666) |
Translation from the Italian text (with help from Google Translate):
Buona sera, Alex; Sul forum Siemens la maggior parte dei membri non parla italiano, quindi abbiamo scelto l'inglese come lingua di scambio. Prova a utilizzare l'inglese o un traduttore elettronico come Google Translate, la prossima volta che ci visita. . Questi sono installazioni completamente funzionali per 21 giorni. Successivamente è necessario acquistare una licenza valida per il prodotto che si desidera continuare. On the Siemens forum most members do not speak Italian, so we have chosen English as an exchange language. Please try to use English, or an electronic translator such as Google Translate, next time you visit us. There are Trial versions of Step 7 (either Step 7 Classic, such as version 5.6, and TIA Portal, such as version 13 SP1) available for download, see the links below. These are fully functional installations good for 21 days. After that you need to purchase a valid license for the product you want to continue with. Note that most documents on the Siemens forum can be downloaded in many languages, including Italian. Where do you procure the current trial software for STEP 7 V5.6? SIMATIC STEP 7 including PLCSIM V13 SP2 TRIAL download Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/25/2017 5:35:09 PMLast edited by: dchartier at: 6/26/2017 2:05:49 PM |
|
7/4/2017 8:14 AM | |
Posts: 7 Rating: (0) |
Thanks , Indra |
9/5/2019 4:20 PM | |
Joined: 9/27/2006 Last visit: 5/4/2024 Posts: 12257 Rating: (2666) |
Hello Eluga; "I need a SIMATIC MANAGER s7 v5.4 basic installer (in your list there is only SP1,2,3,4...) Please update the LINK" I am afraid that there is no link to upgrade. The basic installation of the software version (V5.4 in your case) must always be purchased/licensed. Service packs and Hotfixes can then be downloaded free of charge; but without the original license you cannot install them. Step 7 Classic is now available in v 5.6 SP1, and a trial (21 days activation) can be dowloaded here: https://support.industry.siemens.com/cs/ww/en/view/109761679 Step v5.4, relaeased in 2006, was classified as Discontinued in 2010, when Step 7 v5.5 was released. In the attached screenshot you will find a notice of discontinuation for v5.4, which means it could still have been ordered until 2011. Later it was classed as a product in "end-of-production" phase, which means not available through normal channels any more. https://support.industry.siemens.com/cs/ww/en/view/44370501 If you absolutely need an original v5.4 for your projects, I can only suggest you contact your nearest Siemens rep (seen the link Contact & partners at the right of this page if you need to locate the closest vendor) and ask if they can locate an original CD and license package for v5.4. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/05/2019 16:38:45Last edited by: dchartier at: 09/06/2019 01:09:49 |
|
Follow us on