6/28/2017 6:42 PM | |
Posts: 4 Rating: (0) |
Hi Ahmed,
check the previuos post attacment, it's there.
well I tried it and it work. BUT, 1) according to this post and several others the fix to TON is to assign an explicit coil in Q. 2) I have in the same FB some TON with coils at the output, and some other with a contact reading Q, and all work. Although, is true that the one I presented in my former messages only work with the second approach. Therefore, I only can conclude that is not deterministic how TON works, which is quite dangerous considering that this will control some factory. I attached the complete code so you can see all the variants. Regards, Joaquin |
6/29/2017 11:33 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
This link says it all:
|
science guy |
|
Follow us on