2/18/2017 10:40 AM | |
Joined: 1/9/2017 Last visit: 3/16/2022 Posts: 2 Rating: (0) |
Hello, I have problem with HSC on S7-1200. I made application with HSC1 counting impulses from encored. I download it in CPU and it works. When I power down PLC and when I power up PLC again, I got a message that some hardware is missing (HSC1). Error LED is on. I cant change mode to RUN. Diagnostic buffer is in attachment. When I download hardware configuration and made MASTER RESET, ERROR LED is OFF and I can start PLC. After that application is working good. But it happened every time when I turn OFF and turn ON PLC. Did someone have same problem? Any help is welcome. Djordje AttachmentDiagnostics.txt (216 Downloads) |
6/28/2017 7:00 PM | |
Posts: 1 Rating: (0) |
Hi friend, I have the same problem with HSC using that PLC 6ES7 214-1AG40-0XB0 Have you already got any solution? It could help me a lot. |
Follow us on