7/18/2017 12:20 PM | |
Posts: 3093 Rating: (322)
|
How do you use the blocks for MODBUS/TCP communication via the integrated PROFINET interface of the CPU in STEP 7 Professional (TIA Portal)? |
This contribution was helpful to1 thankful Users |
7/18/2017 1:33 PM | |
Posts: 3 Rating: (0) |
I don't know, I ask if I can do this , maybe add a module of communication |
7/18/2017 1:41 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665) |
Hello Sailouhi; Kaulquappe's answer is a link to a document that answers your original question, not a flippant answer. Double-click on the link, you will be taken to a FAQ that states (amongst other things): This entry gives you sample applications for Modbus/TCP communication via the integrated PROFINET interface of the S7-300 and S7-400 CPUs as well as the IM 151-8 PN/DP CPU in the TIA Portal. Instructions Note Hope this helps,
|
Last edited by: dchartier at: 7/18/2017 1:42:25 PM |
|
This contribution was helpful to2 thankful Users |
7/18/2017 1:51 PM | |
Posts: 3 Rating: (0) |
Sorry i didn't see the link Thanks for the help. |
Follow us on