7/25/2017 9:01 AM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello maybe I have an alternative for you called PC Based Solution. Here you can use an Siemens PC (IPC) with an SPS (Software Controller) and HMI at one PC. On the PC you can Install a Database. And with the SoftwareController you can log your historical data into the Database. 109479140 |
7/25/2017 9:33 AM | |
Joined: 11/28/2012 Last visit: 6/19/2024 Posts: 21 Rating: (0) |
Hi CastlerTroy, Thanks for the info but it seems this will only work with an S7-1500 PLC, I'm using an S7-1200 Rootsap |
7/25/2017 2:51 PM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1733)
|
Hello Rootsap use the following FAQ to create a Copy of your Log to the network path and use the scheduled Task to trigger. https://support.industry.siemens.com/cs/ww/en/view/63042926 Or you use long time Archiving: https://support.industry.siemens.com/cs/de/en/view/109477071 To Edit a date use a script with the Object "Now" and you can use the Time Functions to generate a timestamp like: dim ts ts = Year(now) & "-" & Month(now) & "-" ...... and so on |
Last edited by: Murof at: 7/25/2017 2:53:47 PMLast edited by: Murof at: 7/25/2017 2:54:06 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on