7/25/2017 11:08 AM | |
Posts: 5 Rating: (0) |
Dear all, I have configured a new OS- Client PC. But i have issue that the faceplate for motor, valve, PID, operator input cannot show when i press the device(motor, valve, PID,etc) picture. I have 6 OS-clients, only this OS6 (new) cannot showing the faceplate. I have copied all the @***.PDL files manually from window copy-paste, but still exist. (as mentioned in this topic 35939.) Can anyone help? regards, Adit |
7/25/2017 11:14 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, Check if Global Script Runtime is enabled on the OS client project. You can enable this in the WinCC explorer under the project settings, tab Startup. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on