7/25/2017 11:56 AM | |
Joined: 4/8/2016 Last visit: 2/13/2024 Posts: 133 Rating: (45) |
Hello yac, the CPU 6ES7417-4XT07-0AB0 compatible with the predecessor 6ES7417-4XT05-0AB0. The product note also says that it is spare part compatible. So you can use the CPU as spare part. Link to the Product note: You can find more information about deploying new hardware as replacement in the manual "Compendium part D": In Compendium part D is also written, that you can use successor modules in "spare part-compatible operation" if they aren't listed in the manual "PCS 7 - Released Modules" or the PCS 7 Readme. |
Kind regards |
|
This contribution was helpful to2 thankful Users |
7/26/2017 12:14 PM | |
Posts: 31 Rating: (0) |
Thanks 51N3P, I received also the information from Siemens support that the hardware configuration of the project should remains with the old card (4XT05) and the new card can be installed (4XT07). |
This contribution was helpful to1 thankful Users |
Follow us on