8/2/2017 5:34 AM | |
Joined: 8/25/2006 Last visit: 9/22/2024 Posts: 2209 Rating: (278)
|
Hello. You can change byte order using connectors AT/AR at CTV/CRV blocks (address stage 2: 0 or 1). "1": Standard PROFIBUS setting The data are transferred in the ”Motorola format” (most significant byte before the least significant byte) ”0”: Exception setting The data are transferred in the ”Intel format” (least significant byte before the most significant byte). You can also use e.g. function blocks SWB/SBW or CBR.
|
This contribution was helpful to1 thankful Users |
Follow us on