8/22/2017 3:46 PM | |
Posts: 12 Rating: (0) |
Hello everybody: I am developing a OPC UA Client to connect with WinCC Runtime Advanced . When I try to open a Session in the server, I get the exception type BadCertificateUntrusted, whit the message ´Certificate is not trusted´. I copied the certificate generated with the code in C# X509Certificate2 clientCertificate = config.SecurityConfiguration.ApplicationCertificate.Find(); in the certs and privete folders in the path ´ProgramData/Siemens/CoRtHmiRTm/MiniWeb 14.0.1/SystemRoot/SSL/´. Also, I installed my application certificated via MMC in the folders ´Thursted Root Certification Authorities´ and ´UA Applications´. I apreciate some hint with my problem. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/23/2017 2:03:17 PMNew subject after splitting |
|
9/6/2017 9:07 AM | |
Joined: 8/21/2014 Last visit: 4/22/2024 Posts: 948 Rating: (13) |
Closed, because the question was posted twice. The second thread with the subject OPC UA Client BadCertificateUntrusted is published within the conference SIMATIC WinCC (TIA Portal). Best regards The Helping Hand |
My Forum is the place to personalize your profile, |
|
Follow us on