7/23/2017 5:14 PM | |
Posts: 92 Rating: (5) |
Hello Dear Adventures I'm Working On an Old Lathe MAchine, Made by Uk- Beaver Controller: Sinumerik 810 T GA1 6FC31-71-1AAZ Simodrive: 6SC6101-3. I have the Wrong Voltage on Enable Pin ( 63 -G0 Power Card ) 18.7Volt and Green Key lights up. Unfortunately, I can't find the R1 and R 2, What I think got the problem. as the attachment file told. Also, there is an R(reset Pin) can I use that? Pin number 9, Which have to outlast the 24V, just output 18.V. Any Help will be appreciated kindly. Russell Attachment610_DA.pdf (338 Downloads) |
Last edited by: Sky Diver840 at: 7/23/2017 5:15:17 PMLast edited by: Sky Diver840 at: 7/23/2017 5:17:50 PMLast edited by: Sky Diver840 at: 7/23/2017 5:22:02 PMLast edited by: Sky Diver840 at: 7/23/2017 5:36:34 PM |
|
7/23/2017 6:11 PM | |
Posts: 92 Rating: (5) |
Here Is the Picture Of My Simodrive 6SC610. |
Follow us on