8/10/2017 11:56 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi community, I would like to share a .stp and .stl file for a extension frame that you can put between the IOT2000 frame and the two lids in order to add two stacked Arduino shield or a higher one. The .zip file also contains two pictures of the printed frame added to an IOT2000. Best regards! AttachmentExtension_Frame.zip (286 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to3 thankful Users |
9/12/2017 11:27 PM | |
Joined: 12/12/2008 Last visit: 4/18/2024 Posts: 69 Rating: (6) |
Hello, Nicely done! Do you know (or could get) the original color code for the IOT2000 housing? I want to get hold of a filament that is exactly or close to the color as possible. Preferably PETG. I can not find the color code on google or any place.... /Ben Also added a proposal for Siemens to make a general top lid with terminals. I dont know if such proposals is considered(?) |
Last edited by: Ben1902 at: 9/13/2017 12:23:38 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on