9/25/2017 8:09 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
what is PLC_3? Is PLC_3 a real PLC? SIMOSIM can't connect to any external PLC! and only one SIMOSIM can be running! |
9/25/2017 8:13 AM | |
Posts: 305 Rating: (1) |
lookat the picture ,PLC_2/PLC_3 all is SIMOTION , i SIMULATION is PLC_3 ,but connect ,all is find PLC_2 ? how can i to connect PLC_3 ? |
9/25/2017 8:17 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
close simosim, select the PLC_3 in the project and start the simosim with the PLC_3 |
9/25/2017 8:30 AM | |
Posts: 305 Rating: (1) |
this idea is not connect PLC_3. i test PLC_2 change IP not the same SIMOSIM, PLC_3 change Ip the same , is OK... |
Follow us on