10/19/2017 4:55 AM | |
Posts: 4 Rating: (0) |
TIA PORTAL V14 / SIMATIC S7-1500 / CPU 1513-1 PN / 6ES7 513-1AL01-0AB0 (V2.1.0) Hi. Since I have managed to have my system online, I have the following problem: My CPU is always kept in the RUN state, but at moments the fault LED starts blinking. It is always due to the loss of communication with any of the stations, but it is always one of the GSD Device type stations. The stations in my configuration of this type are ABB frequency inverters, Cavotec System and a Murrelektronik station. Always, when one fails, the others start to fail, but they are always the same, Siemens stations never fail. I have updated all the GSD Files and I've updated the CPU Firmware but no changes. Can someone please give me some light on this? Thanks in advance. Diagnostics buffer of the module PLC_CPU [CPU 1513-1 PN] AttachmentDiagnostics10192017.txt (185 Downloads) |
Last edited by: Jen_Moderator at: 10/19/2017 11:54:26 AMDeleted Diagnostics buffer, because it already is added as an attachment. |
|
Follow us on