10/19/2017 12:41 AM | |
Joined: 3/30/2015 Last visit: 3/7/2024 Posts: 70 Rating: (1) |
Good day guys, please what can I do in the case of trying to use a different marker from what has been used in an existing program. For example, i have an existing program which i want to incorporate a PUT-GET function into. The program has its Clock memory set at 0. I want to use M10.6 or M255 as the input REQ whenever there is a positive edge. That would require that I change the CPU clock memory to 10 0r 255. Will there be any effect on the other program function in the program? How best can i achieve this? Also, I want to set a Marker bit to be always ON or always OFF or to set a call for an FB in OB1 to serve as the EN, ENO and INIT_COM. Please how can I do this? All the M0.0 to M0.7 have been used. I have attached a screenshot. Thank you. David ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/19/2017 11:35:16 AMNew subject after splitting |
|
10/19/2017 11:36 AM | |
Joined: 6/19/2017 Last visit: 4/18/2024 Posts: 7951 Rating: (162) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on