10/13/2017 9:01 PM | |
Posts: 241 Rating: (1) |
hi what is plc fault contact? |
10/18/2017 2:23 AM | |
Joined: 7/2/2016 Last visit: 6/18/2024 Posts: 120 Rating: (29) |
Hello hamed12580, Siemens PLC do not have a native specific fault contact, but you can create one easier. see the attached file and the video example... is very simple, when any fault ocurrs the CPU will go to stop and OB1 stop too and one bit "always true" assigned for a physical output will falls. Note: its occurs if you don't use the fails OB's, however if you use that OBs you can create reset into those.
sorry my english on the video... |
hope this help, if it was helpful please rate the post! |
|
This contribution was helpful to1 thankful Users |
10/29/2017 5:51 PM | |
Posts: 241 Rating: (1) |
very very good thx |
Follow us on