10/23/2017 12:26 PM | |
Joined: 10/11/2006 Last visit: 3/28/2024 Posts: 5799 Rating: (785)
|
Hello, 5.2.2 Support through the "SINAMICS XML Parser" Duplicate error numbers in the XML file are marked with an “X” as “Duplicates” in the first column of the CSV file when exporting them via the “SINAMICS XML Parser”. 5.2.3 Removing duplicate error numbers To be able to use the warning and error messages in STEP 7 or WinCC, all rows marked with an “X” by the “SINAMICS XML Parser” have to be checked after importing them into Microsoft Excel. Further possibilities: Messagehandling has a template for WinCC. https://support.industry.siemens.com/cs/ww/en/view/51339107 ProjectGenerator_V1_4_3\SIMOTION\EquipmentModules\V5_1\Messagehandling_LMsgHdl\Data\... |
With best regards, |
|
Follow us on