10/24/2017 5:05 PM | |
Joined: 8/9/2016 Last visit: 8/29/2024 Posts: 70 Rating: (0) |
hello all, I've an s7-1500 module {AI/AQ 4xU/I/RTD/TC / 2xU/I ST (6ES7 534-7QE00-0AB0) }. I want to have it configured for 2 wire resistor. The connections for resistors are in attachment. pin 3 with 7 and 4 with 8 are shorted. The two wires for sensor are taken from pin 7, 8. However, I get an input of 32764 (maximum Analog input value) for the tag, and the values does not change with change is resistance. The multi-meter shows the change in resistance as temperature varies, which is a confirmation that the sensor works fine.. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/25/2017 12:40:36 PMNew subject after splitting |
|
10/24/2017 5:06 PM | |
Joined: 8/9/2016 Last visit: 8/29/2024 Posts: 70 Rating: (0) |
hardware configuration |
10/25/2017 8:36 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, do you have a PTC resistor, as you projected? have a look in the manual, how to handle it with PTC-resistors, or in the attachment. hope this helps, regards, AttachmentSpecial features for the use of PTC resistors.pdf (220 Downloads) |
FCK WAR! |
|
Follow us on