8/4/2017 10:14 AM | |
Posts: 14 Rating: (9) |
Hi, I created a Webinterface for the IOT2000, that allows you to:
It may be useful, if the IOT is not in eye range, for debugging, for demonstrations and for developers who want to implement their own server application on the IOT and need help getting started. The server application is executed by node.js, which is already installed in the example image V2.1.3. Here is how you can set it up:
Please be aware that this Webinterface is in early development stages and may not be programmed perfectly. I am grateful for feedback, error reports and ideas what one might add to the webinterface. Feel free to use it for own applications. AttachmentWebinterface.zip (1005 Downloads) |
This contribution was helpful to5 thankful Users |
8/4/2017 10:17 AM | |
Posts: 14 Rating: (9) |
For more information on how the webinterface looks, how to set it up, how it was realized and how you can realize your own server application check out the documenation in the attachment.
Attachmentwebinterface_application_example.pdf (1699 Downloads) |
This contribution was helpful to3 thankful Users |
10/25/2017 10:56 AM | |
Posts: 531 Rating: (34) |
What kind of webserver is this. Does it have any security features or can be bind to a specific network only? |
10/25/2017 2:40 PM | |
Posts: 52 Rating: (2) |
Node JS Webserver, created with the 'express' function of Node JS. More security features that can (and should) be realized are discussed here: Hope that helps a little bit. |
This contribution was helpful to1 thankful Users |
5/22/2019 2:55 PM | |
Joined: 6/17/2014 Last visit: 10/27/2021 Posts: 77 Rating: (0) |
Hi Felixxx, Your web interface works very good. Can we run this automatically on start of the IOT ? Thanks |
5/22/2019 3:23 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Yes, check out this thread on how to run a script at start up. You can then call
Within the script. Kind regards! |
Follow us on