10/30/2017 9:48 AM | |
Joined: 3/2/2015 Last visit: 2/29/2024 Posts: 45 Rating: (5) |
Dear All, In my Project am using Siemens DBA AS to OS Compilation Utility tool to populate the structure and to configure all messages. On the other hand OS is connected to HIMA OPC Server. After compilation Data transfer between OS and OPC Server is healthy but only issue is Messages are not getting triggered which is a internal function as I Guess. .EventRaw#1 is the internal tag which is triggered by External tag called .ALM. For testing I made .ALM tag as internal tag my alarms are triggered but if I make it external which is supposed to come from OPC Server, Alarms are not functioning. I have also attached the screenshot for the type and Message configuration. Give me some suggestions so that I can resolve this issue. Thanks in Advance, Vinoth Loganathan AttachmentDBA.zip (99 Downloads) |
Follow us on