11/10/2017 9:39 PM | |
Joined: 1/21/2010 Last visit: 2/28/2024 Posts: 15 Rating: (1) |
Hi, I have exactly the same problem with the wireless connection, the mentioned service is running but anyway I restarted it. I have TIA Portal v13 SP1 update9, Windows 7, no firewalls and no antivirus running. My TIA portal doesn't find anything, no errors, same massage nothing found. I can ping all the devices on the network fine. I am using an access point connected to the wired network, a colleague also connected wirelessly to the same AP and with same Tia Portal version and he had no problems, everything detected. So it is not the access point. By the way if I change to wired network I can detect all nodes, and everything works fine. But I need to connect wirelessly ! And ideas ? ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 11/13/2017 12:03:03 AMNew subject after splitting |
|
Follow us on