11/17/2017 1:32 PM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22369 Rating: (3012)
|
Hello, download Proneta and check if this tool find the PLC, then assign a IP to it. It can be that you can't use the new S7-1200 with TIA V12, because the old TIA Version doesn't support the newer S7-1200 Types. Which S7-1200 you have exactly (Ordernumber?) and which FW is on it.
|
This contribution was helpful to2 thankful Users |
11/17/2017 8:36 PM | |
Joined: 2/10/2016 Last visit: 6/13/2024 Posts: 115 Rating: (0) |
Dear sir, Thanks for you support.
|
Last edited by: Habeib_nader at: 11/17/2017 8:39:11 PM |
|
11/17/2017 8:48 PM | |||||||||
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, 1-Kindly have a look at the following topic:
|
||||||||
Last edited by: Jen_Moderator at: 11/20/2017 10:35:06 AMInserted right links. Eng.Mohamed Ibrahim |
|||||||||
This contribution was helpful to1 thankful Users |
11/17/2017 10:08 PM | |||||||||
Joined: 7/7/2010 Last visit: 9/23/2024 Posts: 15214 Rating: (2417)
|
If you purchase a V14 license, you can use V11, V12, and V13 in addition to V14 from that one license. The upgrade license migrates your legacy step 7 license to a currently supported TIA Portal (V14) version of TIA Portal. I do hope you consider a V14 license. It can program the older hardware without crashing nearly as much as the older software. V14 also has the benefit of built in support for much more hardware.
|
||||||||
science guy |
|||||||||
This contribution was helpful to2 thankful Users |
Follow us on