11/21/2017 4:47 PM | |
Posts: 3 Rating: (1) |
Hello, I have problem with PLC SIM V14 as well. My problem is different : the communication between PLC Sim and the Runtime doesn't work. My PLC SIM works fine : The PLC CPU 1515-2 PN is correctly simulated But I have no communication when I start the Runtime. I was in V13 so I Win CC Runtime Advanced is now in 14.0.1.0 I'm using Windows 7 Pro x64, Step 7 Pro V14, WinCC Advanced V14 and PLCSIM V14 I guess that my problem is coming from my PG/PC interface : which one should I choose? If you know which one is working plz tell me Thx Victor ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/22/2017 10:38:00 AMNew subject after splitting |
|
11/21/2017 5:19 PM | |
Posts: 3 Rating: (1) |
Thx for your reply I choose the PG/PC interface you said but It's still the same Yes I have updated the HMI in the project to the Version V14. |
11/21/2017 5:34 PM | |
Posts: 3 Rating: (1) |
PROBLEM SOLVED I have removed the PLC password in the connections and it works fine Thx for your help |
This contribution was helpful to3 thankful Users |
Follow us on