11/21/2017 6:13 PM | |
Joined: 1/31/2011 Last visit: 3/15/2024 Posts: 4 Rating: (0) |
Hi all. I have a S5-115 with an IM308B. I need to put on the net (DP profile) an DP/DP coupler. In the DP/DP Coupler User Description Version V1.1b 11/1998 appendix "12.2 Appendix B - Type File" there have type file. I tryed to copy the contents of this appendix and paste into a new text file, saving it as "SI8070AX.200". I'd copied this file into COM ET200 directory together with other .200 files. Opening COM ET200, when configuring a new station, the new component not appear in the choice menu. I discovered that the last character before the ".200" must be the language identification letter (D, E, F, I, S), and the character before the language identification must be "T" letter. The other 6 characters can be anything. Then, I renaming the file as "SI8070TE.200" (in this case needs to work in English), "DP-Gateway" appears in the choice menu, but trying to select it, the error "File Too Large" will appear. Some idea? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/22/2017 10:49:09 AMNew subject after splitting |
|
Follow us on