11/22/2017 3:24 PM | |
Joined: 9/23/2005 Last visit: 5/8/2024 Posts: 4528 Rating: (698) |
Global device vars are seen as DB0. Have a look at this thread. |
Regards, |
|
This contribution was helpful to1 thankful Users |
11/23/2017 6:00 AM | |
Posts: 17 Rating: (0) |
Sorry, but I do not see the addresses, but only the names of variables, maybe I'm doing something wrong? I watch the program via SIMOTION SCOUT. |
11/23/2017 11:09 AM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Hello, it is possible to use TCP/IP communication (LCom). https://support.industry.siemens.com/cs/ww/en/view/51339107 |
With best regards, |
|
11/24/2017 7:18 AM | |
Posts: 17 Rating: (0) |
I did as you said, as I understood in the file OPC_Data.ati there are variables and their addresses in the controller memory. But I can not decipher there most likely ASCII to HEX or something like that. Could you, by the example of one variable, show how to decode its address in memory? For example, "Stat_cycle_counter".
Attachmenttagfiles.zip (104 Downloads) |
Follow us on