12/14/2017 10:52 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, You can find the missing packages as follows: 1. Go to Simatic Manager and open the multiproject 2. Go to the AS project where you want to edit 3. Right click on the AS project in Component View 4. Select Object Properties and open tab: "Required Software Packages" and see what is missing. But, you get the error when creating a new project right? So the project is not created? If so, please post a screenshot of the installed software: 1. Go to Start->All programs->SIEMENS->SIMATIC->Installed software (please not that the file directory can vary between PCS7 versions). The program is located under: "C:\Program Files (x86)\Common Files\Siemens\S7AVERSX\s7aversx.exe". 2. Export the tab: "Products"
|
Last edited by: Oreca at: 12/14/2017 10:56:37 AMIf I could help you, you can use the RATE button. Thank you. |
|
12/14/2017 12:47 PM | |
Joined: 3/2/2007 Last visit: 4/23/2024 Posts: 928 Rating: (5) |
Kindly, check attached file of Installed Softwares. Thank you
AttachmentInstalledProducts.xlsx (87 Downloads) |
... thank you ... |
|
12/15/2017 6:53 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi Ziemens, I cross checked the installed software with my V8.1 version. All components are installed... Very strange...is this a new machine or did you do projects on this ES before? Can you open the APL example project? 1. Go to Simatic Manager, click on File->Open 2. Select column Sample projects and open: "APL_Example_EU". Did you also check where it goes wrong? For example, try to create the project without a SFC and CFC chart and without a PCS7 OS station/Batch/Route control station. When succeed, try to add CFC and SFC and PC station...maybe you get additional errors... |
Last edited by: Oreca at: 12/15/2017 6:54:56 AMIf I could help you, you can use the RATE button. Thank you. |
|
12/15/2017 9:47 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Ahh yes... The CPU410-5H is originally released for PCS7 V8.1 and higher. Since you are using V8.0, you will need a HUP: Hardware Upgrade Package, which Siemens made available. This HUP is available under the following link: CPU410-5H HUP |
Last edited by: Oreca at: 12/15/2017 9:48:59 AMLast edited by: Jen_Moderator at: 12/15/2017 10:48:08 AMInserted right link. If I could help you, you can use the RATE button. Thank you. |
|
12/19/2017 8:34 PM | |
Joined: 2/29/2016 Last visit: 3/12/2024 Posts: 100 Rating: (1) |
Good info! Im working with 410, but its a special one that cpu.. Not as easy as previous cpus |
Follow us on