12/15/2017 9:54 AM | |
Joined: 3/24/2016 Last visit: 8/1/2024 Posts: 4 Rating: (0) |
I would like to know more about this too. Can someone share his or her thoughts about this? Thanks in advance! |
12/15/2017 1:53 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello rv; I do not understand why the original poster would make such a statement, with all the ressources on the forum's Product Support pages it is very easy to locate information on any type of hardware from Siemens Industry. What's more, Siemens support is available locally through Siemens reps, who would have clarified the existence of failsafe modules for these 2 families of distributed I/Os. For example: https://support.industry.siemens.com/cs/fr/en/view/78618356 https://support.industry.siemens.com/cs/fr/en/view/109482397 Hope this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 12/18/2017 8:45:04 AM |
|
12/15/2017 6:05 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello rv: I regret to say that I had misread the original post , and missed the "failsafe analog module" portion of the question. And you (and the original poster) are correct: failsafe analog modules (F-AI and F-AQ) are not presently available for Et 200MP and ET 200SP Profibus slaves. One possible alternative (while we wait for Siemens to provide analog F-modules for the S7-1500 and its distributed I/O) could be found in the ET 200iSP, which supports failsafe I/Os, including an analog input module, and connects to Profibus over an IM 152 http://w3.siemens.com/mcms/distributed-io/en/ip20-systems/et200isp/Pages/default.aspx I have attached a scrrenshot showing the F-AI module vailable in the ET 200iSP. Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on