1/6/2018 5:27 PM | |
Joined: 10/4/2015 Last visit: 6/20/2024 Posts: 1 Rating: (0) |
Hello Dear all All Experts, I am also facing the same problem with CPU 1512 SP-1 PN ( 6ES7 512-1DK01-0AB0 ). I had configure the hardware & download with get/put check box clicked. Now i am unable to download the program . The cpu is in maintenance mode. When i removed the memory card from cpu, then I can see the load option during download, but program cant downloaded due to no memory card. The attachment is attached.Please help me what to do to solve the problem. Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/7/2018 12:10:16 PMNew subject after splitting |
|
Follow us on