1/21/2018 4:06 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, I had done a project over 10 years ago between an S7 300 and a PC to display data from the S7 300. I had used the CP5611 via Profibus and installed the SOFNET S7 if I remember correctly. you must perform a configuration in a NCM --> CP5611 and OPC server, you must also create an S7 connection in Netpro with an unspecified partner with the Profibus address of the S7-300 CPU (pay attention to address details), then you could check with OPC scout. How do you configure an S7 connection for the SIMATIC NET OPC ... |
Last edited by: Jen_Moderator at: 1/22/2018 2:09:47 PMInserted right link. |
|
Follow us on