1/21/2018 6:26 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello,
Perhaps the following topics might help: 1-Tag Converters for WinCC flexible 2-TagConverter for WinCC (TIA Portal) By the help of WinCC TagConverter you import Tags on a easy way from different PLC-editors to WinCC (TIA Portal) |
Last edited by: Jen_Moderator at: 1/22/2018 1:17:08 PMInserted right links. Eng.Mohamed Ibrahim |
|
This contribution was helpful to2 thankful Users |
1/21/2018 6:27 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello MirNa; A few questions: - what A-B PLC model do you have, and what software are you using to program it? - what model PanelView do you use presently (and want to change)? - are you planning to change the CPU and panel, or do you only want to connect a new (Siemens) operator panel in place of the existing PanelView? - when you mention a WinCC project, do you mean a WinCC Flexible 2008 or WinCC TIA Portal v 1x (with an operator panel), or do you mean WinCC v7.4 SCADA? I know it can be confusing, so if this is not clear please say so, we can clarify the issue. As an example, here are the A-B protocols and PLCs supported with WinCC Flexible 2008 on a Siemens operator panel. https://support.industry.siemens.com/cs/ww/en/view/18797249 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/21/2018 6:28:36 PMLast edited by: Jen_Moderator at: 1/22/2018 1:18:17 PMInserted right link. |
|
1/26/2018 9:03 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi You have several choices: -Change the CPU, because only SLC 5/05 have ethernet -Setup RSLinx as OPC Server. Then you can add OPC Driver from WinCC -Add Gataway from Prosoft AN-X2-AB-DHRIO and then you have ethernet. |
Last edited by: JM76 at: 1/26/2018 9:18:24 PMAdd more information If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
1/27/2018 6:37 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi As far I know, there isn´t any tool to migrate AB to WinCC. You can use the above tools, and then you can edit the excel and import to WinCC. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on