2/17/2018 4:28 PM | |
Joined: 5/14/2009 Last visit: 4/23/2024 Posts: 64 Rating: (1) |
This is an ET200SP io drop for the S7-1214 PLC |
2/18/2018 6:46 PM | |
Posts: 2826 Rating: (684) |
Hello.
How do you want to use this? What type of motion control do you have in mind for the S7-1200? (opinion / guessing) BR Attachmentpictures.zip (256 Downloads) |
Last edited by: #dP at: 2/18/2018 6:47:50 PMinline pictures failed - moved to ZIP |
|
This contribution was helpful to1 thankful Users |
2/18/2018 7:05 PM | |
Joined: 5/14/2009 Last visit: 4/23/2024 Posts: 64 Rating: (1) |
Yes. the signal output +-10V goes to an old Simodrive 611A. Encoders are 5V RS422 A B N |
Follow us on