2/15/2018 12:36 PM | |
Posts: 7 Rating: (0) |
Hello, i have question about connecting my PLC (1200 or 1500) directly to the SQL (MSSQL or MySQL). I have read topics like wishlist: tiny sql client , how to fetch data from database and SQL with Simatic 1200/1500 . I have try some examples from web. Some of them don't work, don't have reguested functions or they are too expensive. But i was interested in simatic ODK 1500s SQL Driver or WinCC runtime - will it work without any PC? Just on PLC? I need SQL statemens like INSERT and SELECT, but it will be great when there is UPDATE too. The main condition is to communicate straight from plc without using a PC, so OPC and other PC based solutions are out...(We already using OPC to communicate with PLC and database, but due to so many windows updates, bugs etc we have to remove them from our system) Thanks for response, |
This contribution was helpful to1 thankful Users |
2/15/2018 2:42 PM | |
Posts: 531 Rating: (34) |
Did you check this option? https://support.industry.siemens.com/cs/ww/en/view/109479140 |
Last edited by: Jen_Moderator at: 2/16/2018 9:47:46 AMOptimized link. |
|
2/18/2018 6:36 PM | |
Posts: 2826 Rating: (684) |
Hello.
Is that not for a soft-PLC? (software driven PLC running on a PC) BR |
2/18/2018 10:43 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello; One option found on the web: http://plcsql-link.com/product Facts about PLCSQL Link
There is a pricelist on the website. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/18/2018 10:56:12 PM |
|
This contribution was helpful to3 thankful Users |
12/2/2018 10:10 PM | |
Joined: 8/22/2016 Last visit: 4/15/2024 Posts: 35 Rating: (8) |
Hello Jakub, see my response in different thread: Write data from PLC to the InfluxDB. Originaly it was my respond to your question few days ago, but it was incomplete and therefore has been split. Now I have a solution and everything seems to be running, so I guess, that it could be helpfull also for you. Josef |
This contribution was helpful to2 thankful Users |
7/23/2019 7:00 AM | |
Joined: 2/3/2012 Last visit: 3/18/2024 Posts: 2 Rating: (0) |
Here is the user guide for the SQL Library for S7-1200 / 1500 |
7/5/2020 12:16 PM | |
Posts: 4 Rating: (1) |
Dear All, I was successfully testing the connection between MS SQL to S71200 and s71500 as the following support from SIOS: https://support.industry.siemens.com/cs/ww/en/view/109779336 Lets share the sample project, its very interesting for data logging from S7 PLC to SQL |
Last edited by: Jen_Moderator at: 07/06/2020 09:57:34Optimized link. |
|
Follow us on